详细信息

25. 11월 2009

HARTING innovations on display at the SPS/IPC/DRIVES exhibition in Nuremberg

Philip Harting, Board Member Connectivity & Networks

At this year’s SPS/IPC/DRIVES exhibition, taking place in Nuremberg from November 24 to 26, the HARTING Technology Group is once again showcasing innovations that impress with their future viability, high levels of user-friendliness and outstanding customer benefits.

Especially in economically challenging times, it is essential for industrial companies to achieve utmost process efficiency in connection with consistent, systematic process optimization. The HARTING Technology Group develops key technologies to meet these requirements, and provides solutions for manufacturing companies that offer significant performance reserves for future applications in a sustainable manner.

With its new Ha-VIS preLink technology HARTING has created the option of deploying standardized cabling in all company areas. The preLink connection technology is inserted between the cable termination and the freely selectable mating face. The conventional link is replaced by preLink. Ha-VIS preLink can be used universally with various connectors, such as the RJ 45 and M12, in the IP 20 and IP 67 protection classes, and on both male and female sides of the connector.
This significantly reduces planning costs, installation time and error probability.

HARTING Automation IT solutions provide a uniform communication platform for all in applications in manufacturing companies. HARTING has developed a new switching technology to achieve the required performance level, whereby the switch ensures determinism without the need for special chips in the network devices. This technology earned HARTING a nomination for the Hermes Award, the prestigious, highest endowed technology prize, at this year’s Hannover Messe trade fair. HARTING is presenting the new switching technology’s first series product at SPS/IPC/DRIVES 2009.

“Our objective is to provide customers with dependable, ongoing support, irrespective of the current economic climate, by delivering a constant stream of innovations. This requires precisely the entrepreneurial spirit that has always been the cornerstone of our company’s success,” said Philip Harting, Board Member Connectivity & Networks at the HARTING Technology Group, highlighting the significance HARTING accords to innovation leadership.

har-speed M12 connectors now available for fast Cat. 6 transmission HARTING RJ Industrial® 10G – The new field-installable RJ45 plug for 10Gigabit EthernetShip approval for Ethernet switches according to DNVHan® Q 4/2 now also available with wiring technology for field assemblyCreating links before the links - HARTING Ha-VIS preLink®