详细信息

19. 6월 2017

GERRY WEBER OPEN: 25th anniversary tournament with HARTING connectors

Detlef Sieverdingbeck (left) and Stefan Olding (right), both HARTING Technology Group, and Stephan Pumpe from Marketing of GERRY WEBER WORLD are satisfied with the cooperation

Han-Eco® in the umpire's chair ensures clear decisions on the Centre Court.


The Han-Eco® connectors will be installed in the umpires' chairs and used in the matches between the first-class players at the tournament.

The HARTING Technology Group will be playing its part in the 25th GERRY WEBER OPEN from 17 to 25 June in Halle in Westphalia. As they place their serves, the tennis professionals can be certain that the decisions taken in every match will be completely unequivocal. This is because HARTING Technology Group will be providing the 25th GERRY WEBER OPEN with their Han-Eco®connectors for data, signals and power. The Han-Eco® connectors will be installed in the umpires' chairs and used in the matches between the first-class players at the tournament.


The GERRY WEBER OPEN has been one of the most important and prestigious tennis tournaments in the world since its launch in 1993. Even in its first year, it attracted an audience of around 85,000 to watch exciting volleys on the Centre Court in the GERRY WEBER STADIUM, which is also used for other major events throughout the season. Last year, a total of 111,000 people watched some thrilling world-class tennis; the audience at the final of the ATP tournament alone numbered 11,500. The total prize money for 2017 amounts to over €1.8 million.  

The Han-Eco® connectors will be installed in the umpires' chairs and used in the matches between the first-class players at the tournament.

"We chose HARTING and the Han-Eco® because the connectors made a good impression on us in every respect: they are reliable, robust and guaranteed to perform well, making them ideal for our tournament," said Stephan Pumpe from the Marketing Department at GERRY WEBER WORLD. The HARTING connectors will be installed in the umpires' chairs and connected directly to their laptops.

The Han-Eco® can be fitted quickly and easily. It is used by the organisers of many broadcast events such as pop and rock concerts, theatre performances and musicals. "We are delighted that with our connectors ensuring supply and communication we will be making a contribution to the smooth running of this leading tournament," said Stefan Olding, Managing Director at HARTING Deutschland GmbH & Co. KG.

Han-Eco®: connectors in high-performance plastic, here with modules for transmitting data, signals and power.

Han-Eco®: connectors in high-performance plastic, here with modules for transmitting data, signals and power.