详细信息

28. 11월 2012

SPS/IPC/Drives 2012 - Innovation on all levels

HARTING press conference at the SPS/IPC/Drives 2012

The HARTING Technology Group's innovations are based on the interplay of industrial trends and customer-specific application requirements.

At SPS/IPC/Drives 2012, the company will be presenting its new products, which cover both individual components and also complex approaches to solutions.

Philip Harting, Board Member for Connectivity & Networks at HARTING:
"In HARTING's Integrated Industry concept, components, solutions, systems and consulting services are combined into an innovation range that covers all levels. Each single level is just as important as the interaction of all in order for us to act as competent partners for our customers." 

Dr. Alexander Rost, Managing Director HARTING Electronics:
Our har-flexicon® satisfies the needs of the miniaturization trend in instrument engineering

"Increasing miniaturization plays a central role in industrial instrument engineering. har-flexicon® offers our customers swift and convenient single strand wiring in a 1.27 mm pitch that features superior stability, a fully automatic equipping process and an especially low overall height of only 5 mm." 

The HARTING M12 in 3D MID is the perfect choice for high data rates
"Applications in industrial automation or railroad technology require components that combine speed, reliability, safety and profitability. The new M12 in 3D MID is a high-tech Ethernet connector for high data rates that offers perfect RF performance and mating reliability thanks to highly precise screening. Moreover, it is especially light: we were able to achieve a weight reduction of 58% here.

Dimitrios Charisiadis, Director ICPN HARTING Electric:
HARTING smart Power Networks create energy consumption transparency

"The transparency of a company's energy flows is the basis for all energy policy decisions. smart Power Networks create this transparency for our customers and provide the database for analyzing energy consumption for a continual improvement process based on ISO 50001." 

Claus Hilger, Managing Director HARTING IT Services:
AutoID is a strategic business segment for HARTING

"We offer our customers complete AutoID solutions that combine consultation, hardware, software and system integration. We are meeting the concerns of this strategic business segment with our new "HARTING IT System Integration" area. 

About HARTING:
Intelligent high-performance connection technology forms the basis of industrial application and product technology. The HARTING range of products and solutions comprises connectors, device connection technology, network components and ready-to-use system cables. HARTING products connect and network devices, machines and facilities via data, signal and power. These offerings enable solutions for the following markets: automation technology, energy, transport technology, radio, stage and event management technology, machine construction, medical technology, embedded computer systems, industry network and infrastructure. HARTING also produces electro-magnetic components for the automobile industry and provides solutions for the fields of housing technology and shop systems.
The HARTING Group currently employs about 3,600 people across its 36 subsidiaries.