HANNOVER MESSE Press folder
All the information about the HANNOVER MESSE, from April 1-5, 2019, is included here.
The HANNOVER MESSE is the most important industrial trade fair in the world. It takes place every spring at the world's largest exhibition grounds in Hannover, Germany.
The HARTING Technology Group is presenting many of its technological highlights at this year's HANNOVER MESSE (April 1-5, 2019, hall 11, stand C15). They are presenting "Intelligente Connectivity" in the spirit of the trade fair's motto „Integrated Industry – Industrial Intelligence“. As a pioneer of integrated industry, HARTING uses digitisation to create added value for customers.
HARTING presents intelligent connectivity at HANNOVER MESSE for the next steps towards the Future Factory
In addition to clear standards for industrial infrastructure, the production of the future requires ever more intelligent systems and processes. The field of activity ranges from the collection of sensor data, analysis in Edge environments or in Clouds, initial results presentations in connection with Predictive Maintenance, and through to Machine Learning and Artificial Intelligence (AI)...
Download press material here:
Injection moulding machine provides reliable product quality data
An ARBURG injection moulding machine at the HARTING stand (Hall 11 / C15) will not only produce plastic parts, but also supply significant volumes of data. In cooperation with ARBURG, HARTING will use this practical example to show how e.g. energy measurements and ambient readings can be used to monitor product quality and signs of wear...
Download press material here:
MICA® as a universal link between machines, cloud and IoT platforms
Data from machines and processes are the basis for performance increases and an optimised material flow. Together with partner companies and customers, HARTING will be at the HANNOVER MESSE (1 - 5 April 2019 / hall 11/ stand C15) to demonstrate how data from processes, sensors and controllers can be used to get the best out of production...
Download press material here:
Small, robust and flexible: Han® 1A
HARTING will present intelligent connectivity solutions for the Cloud, Edge and IIoT at the HANNOVER MESSE trade show. The technology group calls it HAI³ powered Connectivity! In the area of the Edge, HARTING is showing the Han® 1A, which is significantly smaller than its hitherto smallest rectangular HARTING industrial connector, the Han® 3A...
Download press material here:
A clean connection: Han® F+B for the food industry
Food industry players who want to shorten set-up times and production stoppages can do so by using connectors. As a result, HARTING developed the Han® F+B series. The series’ design is intended to provide strong resistance to detergents, functionality in the widest possible temperature range (-40 to +125° C), and to prevent the build-up of dirt...
Download press material here:
Industrial cloud communication gets standardized
Download press material here:
First rear mounting options for Han® metal hoods and housings
Download press material here:
HARTING Technology Group accelerates e-mobility
Download press material here:
Modular storage systems for the industry use Han® interfaces
The Commeo GmbH from Wallenhorst near Osnabrück has developed a modular energy storage system that allows applications from mobile robots to the power supply for industrial plants and factories to run securely and uninterrupted. The Commeo units can be used as an emergency power supply or as a buffer to the mains that provides compensating power when required...
Download press material here:
HARTING RJ Industrial®MultiFeature series now even easier to assemble
Download press material here:
Single Pair Ethernet key technology for the factory of the future
The Industrial Internet of Things (IIoT) is growing at a rapid pace. Experts agree that Single Pair Ethernet (SPE) will be one of the key technologies that will significantly shape the success of the IIoT. The factory of the future needs high data streams – and for this, the industrial sector needs connectivity which adapts itself to increasingly growing demands...
Download press material here:
Press Contact
HARTING Stiftung & Co. KG
Detlef Sieverdingbeck
General Manager Communication and Public Relations
Marienwerderstr. 3
32339 Espelkamp
Tel.: 05772 47-244
Fax: 05772 47-400
Detlef.Sieverdingbeck(at)HARTING.com