2. News
  3. Optimised current carrying capacity: Bridge to the electric future
tec.news
31 March 2025
3 minutes

Optimised current carrying capacity: Bridge to the electric future


Improving the efficiency and performance of electrical connectors for the manufacturing industry
Optimised current carrying capacity

The manufacturing industry is faced with the challenge of adapting its systems to increasing performance requirements – without claiming more space. Find out here how we at HARTING are improving the efficiency and performance of electrical connections through targeted design optimisations and advanced, leading-edge technologies.

The All Electric Society requires electrical energy, which is supplied by way of the power core both between and within the sectors. In many cases, the transition to electrified systems will entail higher performance levels or new systems with more power will have to be created.

The gains in on-board power in automobiles is an illustrative example from everyday life. This measure simplifies the implementation of so-called "break by wire" and "steer by wire" applications. The former refers to an electric braking system in which the braking forces are transmitted electronically and not mechanically, in other words by way of brake lines. The second refers to an electronic steering system in which the connection between the steering wheel and the wheels is also not mechanical, as with steering rods, but is executed via electrical signals. These performance gains also optimise the charging process for electric cars. Here, large amounts of energy have to be transferred to the vehicle by way of a connector in a short time so that the electric car is as powerful as a combustion engine when "refuelling". Similar examples can also be found in other sectors.

Despite the higher energy requirements, the available space remains unchanged. At the same time, the efficient installation, maintenance or operation calls for the use of connector, which must therefore be able to offer higher current-carrying capacity while retaining the same size.

»

There are three key starting points to improving current carrying capacity: the cable connection, the contact material and the contact point itself.

Stephan Middelkamp

Stephan Middelkamp

General Manager for Qualität and Technologien

The key to boosting efficiency


This is where current carrying capacity enters the picture. It indicates the maximum current that a connector can transmit for a specific cable diameter. This capacity results from the balance between the heat generated due to the electrical resistance and the heat dissipated. The latter is dissipated both by radiation and by way of the cable. While higher current-carrying capacities can be realised more easily with larger connectors and cables, this is not an option in many applications. In some cases, active cooling of the connectors or the use of alternative plastic materials that allow higher temperatures will provide a solution.

Reducing electrical resistance is another alternative, which prevents heat from developing. This also improves energy efficiency. Ultimately, there are three key starting points for improving current carrying capacity: the connection of the cable, the contact material and the contact point itself.

There are various solutions for the cable connection. So-called "crimping", i.e. making a mechanical connection that provides both electrical contact and mechanical strength is a common technique in the energy sector.

A well-executed crimp considerably reduces the contact resistance due to the plastic deformation of the cable and the contact area. The right crimping tool and the correct parameters are crucial factors here. In terms of the contact material, the alloy selected is also of particular interest, as it can significantly increase conductivity. Copper alloy is generally used as the base material.

The resistance in the mating area is influenced by various factors. The number and size of the contact points can be optimised by the specific design: The larger the contact surface, the lower the resistance. The normal force – in other words, the force with which the mating parts are pressed together – also plays a major role in this context. A higher normal force increases the effective contact surface, meaning that more current can flow per contact point, whereby the choice of surface supports this effect. A higher normal force also entails greater insertion force, however, which in turn can increase wear.

Ultimately, it is evident that the optimised design of many parameters improves the overall current carrying capacity. State of the art simulation tools enable us to optimise the current carrying capacity as early as the design phase, meaning that different designs and materials can be selected and adapted accordingly.

Discover all articels of tec.news issue 48
Stephan Middelkamp

Dr. Stephan Middelkamp

Position: General Manager Quality & Technologies

  • Department: SSU QT
  • Company: HARTING Stiftung & Co. KG
[email protected]

Related news


Get involved in shaping the tec.news!
14 January 2026

Reader survey

What do you expect from a technology magazine – product knowledge, trending topics or completely new perspectives? Let us know.
read more
harting-web-header-ethernet-gast-0062-2500x1500px-20251029.jpg
21 November 2025

Ethernet: 50 years old, but still the gold standard

Around since the 1970s, but not a bit tired: how Ethernet keeps reinventing itself and forms the backbone for the latest trends.
read more
Focus on transition
21 November 2025

Focus on transition

Indian Railways is using data to get on track for carbon neutrality and better safety. Powered by HARTING.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590