2. News
  3. The future role of base-load technologies
tec.news
30 March 2025
3 minutes

The future role of base-load technologies


Would they be an advantage for the German energy system in the future?
The future role of base-load technologies

Nuclear fission, natural gas, geothermal energy, nuclear fusion: Would these base-load technologies be expedient for the German energy system in the future? These issues were analysed by the academy initiative "Energy Systems of the Future" (ESYS).

What are base-load technologies?


Base-load technologies are continuously available for power generation. Due to their high investment costs, base-load power plants must be in operation almost uninterruptedly in order to be profitable. At present, nuclear power plants and lignite-fired power plants feature as typical technologies.

In the case of residual load power plants the situation is different: Although these power plants are also continuously available, they only run intermittently, for example when solar and wind energy are not supplying enough electricity. Residual load power plants entail comparatively low investment costs but high fuel costs. Hydrogen-fuelled gas turbine power plants are salient examples of low CO2 residual load power plants.

Possible low CO2 base-load technologies


Nuclear power plants are associated with unanswered questions revolving around costs, safety, final disposal issues and proliferation. Current new construction projects are usually significantly overrunning schedules and budgets.

Natural gas power plants with CO2 capture could probably be realised on a large scale within the next 20 years, while building up the infrastructure for CO2 will represent a challenge.

Geothermal energy has little potential for generating electricity in Germany – here is better suited to providing thermal energy.

Nuclear fusion is not expected to be able to make a significant contribution to the electricity supply until after the year 2045 at the earliest.

Base-load power plants can, but do not necessarily have to be part of the future energy system


The expansion of renewables and the European electricity and hydrogen grids are expected to cover the electricity demand and most of the hydrogen demand within Europe. Nevertheless, base-load power plants could still contribute to the energy supply. The key here is a flexible hydrogen system that enables the power plants to achieve high capacity utilisation. Their electricity could be used for electrolysis in times of low demand and thereby reduce hydrogen imports. However, they hardly impact on the expansion and development requirements of the grids for electricity and hydrogen, and the switch to e-mobility and heat pumps would also have to remain unchanged. Their benefits arise primarily when they are more cost efficient than their alternatives. However, due to their long construction and utilisation periods, new base-load power plants are more of a long-term option.

Base-load power plants do not substantially change the overall costs


The overall system costs of the transition to climate neutrality by 2045 in connection with the expansion of base-load power plants – also under optimistic assumptions – are similar to those in the reference scenario, which primarily relies on the expansion of solar and wind energy. Additional risks notable here: Increased costs and delays in the construction of base-load power plants, both due to the lower level of technological maturity of the respective technologies and the typical complexity of large-scale projects.

Discover all articels of tec.news issue 48
Karen Pittel

Karen Pittel

  • Company: ifo Institute, ESYS Board of Directors
Philipp Stöcker

Philipp Stöcker

  • Company: Philipp Stöcker, ESYS Office

Related news


Get involved in shaping the tec.news!
14 January 2026

Reader survey

What do you expect from a technology magazine – product knowledge, trending topics or completely new perspectives? Let us know.
read more
harting-web-header-ethernet-gast-0062-2500x1500px-20251029.jpg
21 November 2025

Ethernet: 50 years old, but still the gold standard

Around since the 1970s, but not a bit tired: how Ethernet keeps reinventing itself and forms the backbone for the latest trends.
read more
Focus on transition
21 November 2025

Focus on transition

Indian Railways is using data to get on track for carbon neutrality and better safety. Powered by HARTING.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590