2. News
  3. Teamwork relieves stress on circuit boards
tec.news
11 March 2025

Teamwork relieves stress on circuit boards


Fielding the completely revised G-Drives series of drive controllers, Siemens is focussing on a modular concept for all performance classes.
Teamwork relieves stress on circuit boards

Fielding the completely revised G-Drives series of drive controllers, Siemens is focussing on a modular concept for all performance classes. The flexible har-drive system is at work in the new generation of devices, handling the internal transfer of current/power from one circuit board to another. The previous connection of the PCBs involving rigid stand-offs made it a challenge to align them absolutely flat and parallel to each other. The har-drive connectors provide the PCBs with the necessary freedom of movement, while ensuring reliable power transmission.

Revamping the entire portfolio of the SINAMICS-G (General Purpose) series, Siemens has greatly streamlined the complexity of all power classes of frequency inverters thanks to modular design. This has trimmed the number of variants significantly. Necessary adaptive adjustments, such as chokes, can be installed variably depending on the application and the required variant.

A flexible connection of the circuit boards for current/power transmission is one key element of the new development. The har-drive system replaces the former rigid stand-off solutions, which can be challenging when aligning PCBs absolutely flat and parallel to each other. In worst case scenarios, this can lead to distortions of circuit boards, which in turn is detrimental to the correct assembly and heat dissipation of IGBTs, chokes and other thermally relevant components.

The necessary freedom of movement


The entire assembly of large and heavy components such as chokes and filters is facilitated by the fact that complex screw connections in the area of the filters are dispensed with, allowing the integration of more compact designs or more power.

Har-drive connectors are available in various sizes and provide the necessary freedom of movement for PCBs, while ensuring reliable power transmission for all variants of the SINAMICS-G series. Thanks to a maximum horizontal freedom of movement of 3 mm, the connectors are flexible enough to effectively prevent tension within the PCB. In frame sizes A to C, the contacts are bundled in an insulating body, ensuring convenient handling. Single contacts are used from frame size D upwards. In addition to PCB to PCB connections, cable to BUS bar links are likewise an option.

»

The har-drive connection gives the PCBs the necessary freedom of movement while ensuring reliable power transmission.

Rainer Bussmann

Rainer Bussmann

Global Product Manager HARTING Electronics

International teamwork


The terrific international teamwork, enabled by Siemens and HARTING locations in the UK, Germany and China, has impressively demonstrated how combined expertise in device design and industrial connectivity can deliver rapid and series-ready OEM solutions. The very short realisation time, from the initial idea through to the finished product, underlines the dynamic cooperation and keen awareness of the HARTING OEM team in catering to customer requirements.

Marc Genau

Marc Genau

Position: Developer OEM Solutions

  • Department: OEM Solutions
  • Company: HARTING Electronics
Rainer Bussmann

Rainer Bussmann

Position: Global Product Manager

  • Department: PM Circular Interface Connectors
  • Company: HARTING Electronics

Related news


Alpha Centauri Solar Racing: Swiss engineering excellence for sustainable mobility
15 July 2025

Alpha Centauri Solar Racing: Swiss engineering excellence for sustainable mobility

Alpha Centauri Solar Racing, also known as aCentauri Solar Racing, is an innovation project initiated by students at ETH Zurich.
read more
Digitalisation of local network stations (LNS)
11 July 2025

Digitalisation of local network stations (LNS)

The term “smart grid” is no longer unfamiliar and, in short, refers to a digitally based electricity network that is designed to function reliably and as efficiently as possible to ensure security of supply for end consumers.
read more
Swissloop: Innovative spirit and speed meet Swiss precision
24 June 2025

Swissloop: Innovative spirit and speed meet Swiss precision

Swissloop is a student initiative dedicated to the development and research of Hyperloop technology.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745
  • 粤公网安备 44049102496590