Product category:
Smart connectors
OverviewProductsKnowledge
  1. Home
  2. Industrial connectors / Han®
  3. Connectors & cable assemblies for specific applications
  4. Smart connectors
  5. Knowledge

Knowledge about smart connectors


Locking systems for hoods and housings

Locking systems for hoods and housings

The locking mechanisms of hoods and housings do not only protect the connector from unintentional openings, they also increase the tightness. The most often used locking mechanism for industrial connectors are locking levers. However, there are several mechanisms available in different versions, each of which has its advantages and is suitable for special applications.
Learn more
Header_IP-protection_0.webp

IP protection (contact protection, dust, water)

The connector’s housing, sealing and locking mechanism protect the connection from external influences such as mechanical shocks, foreign bodies, humidity, dust, water or other fluids.
Learn more
HARTING_Anschlusstechniken_Coverbild_230502.tiff

Termination technology

The most common termination techniques can be assembled into the Han® connectors. Special inserts and contacts are available to match the particular techniques of wire termination. The choice of the right termination technique depends mainly on the type of cable, the cable cross-section, as well as the number and type of contacts. In addition, all termination types offer different advantages for different production conditions.
Learn more

What are smart connectors?


Smart connectors are connectors with intelligent additional functions that can transport, process, store and forward data to other systems/units. The necessary work is performed by microprocessors or memories on the lower levels of machines and systems. Smart features are used to identify machine parts and ensure safety, e. g. by checking the locking status of the connector, measuring performance and making the measurement results available for predictive maintenance or protecting components against overload/overvoltage.

What types of smart connectors are there?


Smart connectors differ in terms of function and type of intelligent components. Intelligence is being introduced in the form of modules for modular connectors. Another option is to upgrade connectors, housings and/or insulators with sensors and entrust them with additional tasks.

  • Surge protection through modular connectors for electronic end devices

  • Mini-switches/modules integrated in connectors for Ethernet distribution

  • Profinet and CAN ID modules for component identification and decentralised storage of machine-relevant data

  • Status monitoring of voltage, current, power and temperature in the module, generation of data records for condition monitoring, e.g. of the system cabling.

How do smart connectors work?


Smart connectors have sensors, small processors or data storage devices on board, for example. Temperature, current, proximity, touch or force sensors are possible. Properties such as voltage, pressure, current, power or temperature are measured. The sensors are either housed separately in the connector housing, together with small computing units and other electronic components, or they are located in their own modular connector, which is part of a larger interface. The sensor data is transmitted to the system monitoring/monitoring systems via physical cable, WLAN or Bluetooth communication.

Who uses smart connectors where?


Smart connectors are used in mechanical engineering to identify individual processing sections of machines and systems and make them transparent. Specialised connector modules read, write and store data locally and communicate with other industrial-grade components using common protocols. They identify aspects of machine processes and are close to the system parts about which they collect information.

Wherever downtimes with high follow-up costs can occur in the printing or automotive industries, for example, it is particularly important to utilise smart functions. The aim is to avoid failures in advance.

Smart connectors perform their function in a decentralised manner at the lower level of machines and systems. Temperature data, serial numbers of machines and their components, IoT statuses, service life or operating hours, and who was the operator at what time can be documented.

Intelligent connectors can also be used to protect control cabinets in data centers: A miniature fuse in a signal interface ensures that in the event of a fault on an M12 connector, the path to the downstream control system is cut off. A corresponding red LED lights up on the connector.

If a fuse has blown, this can be recognised from the outside by the red light without opening the control cabinet. A defective fuse can be replaced more quickly.

What are the advantages of smart connectors?


Smart connectors are located where interfaces are already planned anyway. The smart additional functions do not increase the space requirement, or not significantly. Smart connectors allow the hardware for system monitoring to be arranged in a decentralised manner, close to important components. This can relieve the burden on centralised monitoring systems for machines and systems. When monitoring system components such as cabling, impairments to the energy supply, for example due to cable kinks, cable breaks or a lack of power supply, can be detected and rectified at an early stage - before costly, time-consuming system downtimes occur. What do I need to look out for when selecting smart connectors?

The connector must be able to use the same protocol as the rest of the system – so that it can communicate with the other components. The data that is collected must correspond to what the machine or system requires.

The temperature limits of the connector must match the temperatures in the system environment.

It can be useful to plan for future expansions and to plan dummies for the modular interface accordingly.

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745
  • 粤公网安备 44049102496590