2. News
  3. Han® Push-In family extended by monobloc insert
Products
14 November 2023
3 minutes

Han® Push-In family extended by monobloc insert


Following on from the market launch of modular push-in inserts this spring, the next expansion stage has now been ushered in: HARTING is expanding its portfolio with a first monoblock variant for the Han®-Compact housing.
Han® Push-In family extended by monobloc insert

Following on from the market launch of modular push-in inserts this spring, the next expansion stage has now been ushered in: HARTING is expanding its portfolio with a first monoblock variant for the Han®-Compact housing.

Thanks to the use of push-in technology, the new Han® Q 8/0 insert enables up to 30 % faster field assembly of connectors. This makes it particularly suitable for environments where space for installation work is at a premium.

Push-in technology is a further development of the cage-clamp. As it makes connection as simple as possible, these inserts are particularly suitable for field assembly, for example in power engineering systems or in the assembly of machine modules or production lines.

The handling of components, for example during maintenance work, is also facilitated. What’s more, a special tool is available for quick disassembly.

If wires with wire end ferrules have been opted for, connections via push-in technology are entirely tool-free.

ix-Industrial.jpg

Thanks to push-in technology, stranded wires with wire-end ferrules can be connected in the Han® Q Monoblock – entirely tool-free.

The use of push-in connections enables stranded wires fitted with wire end ferrules to be inserted directly into the contact chambers. An internal clamping spring snaps shut when the sleeve reaches the bottom of the chamber, thereby ensuring tensile strength. In the case of applications with stripped stranded wires (without sleeve), the pressure of a screwdriver on the orange actuator is sufficient to hold the cage-clamp open when inserting the cable ends.


Thanks to the Han® Q with push-in technology, power and signals up to 16 A / 500 V can be transmitted in the most compact of spaces. A contact chamber is available for the protective ground conductor (PE) - a type of layout frequently opted for in mechanical engineering for connecting motors/actuators...

The advantages at a glance:


  • Cost savings: Assembly times are reduced by up to 30 % thanks to direct insertion of the conductor into the contact chamber

  • Maximum flexibility, as the tool-free connection of stranded wires and solid wires is possible in the use of wire-end ferrules

  • The turn of a screwdriver is sufficient when using stripped stranded wires (without wire end ferrules)

Dirk Teiwes (HARTING)

Dirk Teiwes

Position: Teamleader Heavy Duty Connectors

  • Department: Product Management Heavy Duty Connectors
  • Company: HARTING Technology Group

Related news


Data Centre header background
23 October 2025

Building Smarter Data Center Infrastructure for the AI Age

Serving next-generation, AI-driven applications requires a dramatic rethink of traditional data center design. Data center infrastructure must evolve rapidly – becoming not only larger, but smarter, faster, and greener. Every connection system and square foot now counts in the race to keep up with exponential demand.
read more
Vertiv SmartIT Banner.png
21 October 2025

Vertiv and HARTING Unveil Data Center Rack Power Solution at OCP Summit

HARTING and Vertiv have teamed up to introduce a new rack power solution designed to simplify and accelerate data center deployment. The Vertiv PDB solution was launched at OCP Summit in San Jose, California
read more
Food processing and packaging machinery
29 September 2025

Miniaturisation of production systems: Just how far can you scale down?

In order to minimise the amount of material used and achieve cost savings, machines and other means of production are becoming increasingly compact. This is a trend that can be observed globally. But just how far can the condensation of individual functions and, along with it, miniaturization proceed in a sensible way? From experience and close cooperation with customers from a wide range of industrial sectors, HARTING as a manufacturer of industrial interfaces can share practical recommendations and experience. This enables manufacturers and users of production systems to discover and exploit the enormous potential of miniaturisation.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745
  • 粤公网安备 44049102496590