2. News
  3. M12: PowerX
tec.news
7 March 2025
3 minutes

M12: PowerX


Connectors with enough capacity for the increasing power requirements of applications in all sectors of the AES
M12: PowerX

L-coded and K-coded M12 connectors meet the increasing energy requirements of compact devices and transmit more than 10 times the power of previous solutions, while retaining the same size. They provide up to 7.5 kW supply power in the most compact of spaces - more than enough for compact, decentralised applications in all sectors of the AES. M12 circular connectors are a common standard in many industrial applications when it comes to the robust connection of data and power. Given their international IEC standardisation, PNO conformity and widespread use, they represent an ideal foundation for industrial applications.

Devices and drives in industrial applications are becoming increasingly powerful, while retaining the same dimensions as before. These performance gains are also reflected in the consumption of electrical power, which must be connected by way of a suitable interface. HARTING is meeting this challenge of enabling existing, familiar connection sizes to elevate performance with robust, internationally standardised M12 Metric Circular Connectors.

X-times the power


M12 connectors are a well established interface for the transmission of signals, data and power in industrial applications. The power supply for devices was limited to around 100 W with the existing A, B and D codes. With the K-coded and L-coded connector faces, the M12 size meets the requirements of the AES – thereby offering several kW of transmission power (up to 7.5 kW) in the most compact of spaces. This boosts the possible transmission power in a compact size by orders of magnitude.

In detail:


The 5-pole L-coded connectors can handle an output of 0.75 kW at 16 A in the extra-low voltage range – making the L-coded version highly suitable for field distributor boxes, fieldbus-controlled I/O boxes, power supply units and valve applications. Sub-distribution networks with 24V or 48V working voltage also feature as typical utilisation scenarios. The PNO (ProfiBus user organisation) regards the L-coded M12 Power as the new standard device connection for the power supply of field devices.

K-coded


The 5-pole K-coded connectors transmit up to 630 V and 12 A – covering the typical connection parameters of three-phase motors in the kW range (up to 7.5 kW) – which account for the lion's share of the systems.

Cable assembly or field connection


On the cable side, HARTING is offering field-assembly HARAX® insulation displacement connectors (IDC) and crimp connectors for straight pin and socket versions, featuring a 360-degree hood concept. Consequently, HARTING's M12 connectors are meeting market requirements that extend well beyond the specifications of the relevant IEC 61076-2-111 standard.

Discover all articels of tec.news issue 48
Jonas Diekmann

Jonas Diekmann

Position: Technical editor

  • Department: Global Product Management
  • Company: HARTING Electronics GmbH
[email protected]

Related news


Get involved in shaping the tec.news!
14 January 2026

Reader survey

What do you expect from a technology magazine – product knowledge, trending topics or completely new perspectives? Let us know.
read more
harting-web-header-ethernet-gast-0062-2500x1500px-20251029.jpg
21 November 2025

Ethernet: 50 years old, but still the gold standard

Around since the 1970s, but not a bit tired: how Ethernet keeps reinventing itself and forms the backbone for the latest trends.
read more
Focus on transition
21 November 2025

Focus on transition

Indian Railways is using data to get on track for carbon neutrality and better safety. Powered by HARTING.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590