2. News
  3. One Single Interface for all lifelines
tec.news
5 December 2024
3 minutes

One Single Interface for all lifelines


Current drives and servomotors in industrial applications are connected to the necessary lifelines by way of several interfaces. Data, signals and power are each connected via plug connections that are specialised for their individual task – which costs space.
One Single Interface for all lifelines

Digitalisation and decentralisation, however, mean that the number of smaller drives networked directly via Ethernet is continuously on the rise. New, space-saving concepts that efficiently transmit power and data are, for example, the hybrid interfaces from the One Cable Automation Initiative.

At present, electric drives in industrial applications are usually connected via several interfaces. M23 circular connectors play a particularly important role here, as they offer the necessary stability and shielding properties thanks to their metal housing. The power supply and signals/data are usually connected via separate interfaces, which takes up space on the drive.

The increasing digitalisation and, above all, the decentralisation of production means that large, central drives are on the decline and are being replaced by multiple, smaller counterparts. These can be controlled more individually, while performing the same work with lower power consumption and increasing the efficiency of the entire process.

Rethinking connection concepts


Drive manufacturers are continuously developing their portfolio in this respect and are also focusing on the miniaturisation of their products. The space on drives is contracting, meaning that the connection concepts also need to be rethought. In addition to the power supply, drives require an additional control interface by which signals, BUS or Ethernet protocols are transmitted.

In order to save even more space in the future and reduce the complexity and expense of cabling, the focus is clearly on hybrid connection concepts. These combine the supply of power and signals/data, thereby realising the idea of the One Cable Automation Initiative. The aim here is to ensure that each device is supplied by way of just one central interface, that would ideally be standardised. This saves time during assembly and eliminates the need for countless individual strands.

Transmiting power and signals/data simultaneously


The respective standards for hybrid circular connectors in various sizes are IEC 61076-2-117 and IEC 61076-2-118. The former describes metric solutions of various sizes (M „XX“), which offer a combination of screw and bayonet locking and the second standard (-118) describes the bayonet solutions (B „XX“). They all combine the simultaneous transmission of power and signals/data. There will be a different number of power contacts, combined with two or four control contacts, which transmit either BUS protocols, Single Pair Ethernet (SPE) or Industrial Ethernet.

Standardisation ensures cross-manufacturer compatibility. This creates trust among users who want to have access to second sources and do not have to rely on proprietary solutions.

Rainer Bussmann

Rainer Bussmann

Position: Global Product Manager

  • Department: PM Circular Interface Connectors
  • Company: HARTING Electronics

Related news


Get involved in shaping the tec.news!
14 January 2026 tec.news

Reader survey

What do you expect from a technology magazine – product knowledge, trending topics or completely new perspectives? Let us know.
read more
harting-web-header-ethernet-gast-0062-2500x1500px-20251029.jpg
21 November 2025 tec.news

Ethernet: 50 years old, but still the gold standard

Around since the 1970s, but not a bit tired: how Ethernet keeps reinventing itself and forms the backbone for the latest trends.
read more
Focus on transition
21 November 2025 tec.news

Focus on transition

Indian Railways is using data to get on track for carbon neutrality and better safety. Powered by HARTING.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590