2. News
  3. Standards for individualists, or: What suits my machines?
Products
25 September 2025
6 minutes

Standards for individualists, or: What suits my machines?


One of the most significant challenges in production technology today is the question: how do I meet the "unusual" wishes of end users?
Customised interface solutions for a control cabinet

Robot manufacturer KUKA has formulated a conclusive answer: "The key [to mass customisation] lies in a high degree of standardisation and automation, which at the same time leaves room for variations in customer-relevant product features. The concept of modularisation, which offers customers individual product configuration ... is also a cost-effective way of fulfilling individual customer requirements ..." [1] Individualisation, as it is currently being pursued, is not least one of the core aspects of Industry 4.0.

Interfaces are an important part of modularisation. But do they always have to follow certain standards? The increasing automation and modularisation of production systems bring technical and economic advantages for OEMs and end users. Interfaces are playing an increasingly decisive role in this. The experience of HARTING's customers clearly shows that it is important to differentiate, because in some areas standardised interfaces are more advantageous, while in others "customised" interfaces are better!

In order for OEMs to determine the right degree of customisation for their machines and to reconcile the sometimes conflicting requirements throughout the life cycle, it is helpful to think in terms of different "clusters" or function groups.

Function groups

Developments in electronic components have enabled an enormous consolidation of functions. On the one hand, this technological advance makes it easier to modularise and scale machines. On the other hand, it requires thinking in terms of ever smaller and more elementary functions, and the initial effort involved in developing the systems is growing. Despite these sometimes negative implications, the advantages of customer-oriented customisation outweigh the disadvantages. This is because the appropriate overall arrangement of sensors, actuators and other components, as well as the linking of the corresponding functions, are the absolute domain of OEMs.

There are similarly significant changes here: the enormous increase in performance of technologies for electronic drive control has given rise to new concepts for production plants. This functional group is also one of the core competencies of machine manufacturers.

Manufacturers of production systems are increasingly focusing their development efforts on a few select technologies. However, the generalist perspective remains with the total system suppliers. The question of the right interfaces is particularly interesting for highly specialised technology units. What these have in common is that they are used as finished modules with clearly defined functions and interfaces. The linking of the units forms the central know-how of the OEM, not the components used themselves.

Mechanical engineering specialising in production technology has long been involved in shaping data transmission technologies in the form of industrial bus systems or Industrial Ethernet. However, the possibilities of cost-effective data connection to the cloud are technologically revolutionary. These technologies make it possible to redesign the entire business approach of OEMs. They are not part of their core competence, but they harbour the greatest potential for change in production systems.

Advice for customised interfaces

HARTING's analysis of customer applications has resulted in the following recommendations for customised interfaces:

  1. In general, it makes sense to use customised interfaces for functional groups that represent a large part of the OEM's core competence.

  2. Customer-specific interfaces are most commonly used for modules that are developed or manufactured directly by the respective manufacturer.

  3. Standardised interfaces are usually used for sensors and actuators. However, innovators are certainly trying to set themselves apart from the market environment by using specifically tailored interfaces.

  4. When it comes to data interfaces, mechanical engineering manufacturers rely entirely on standardised solutions. As data transmission technologies are undergoing enormous change, these are largely determined by the suppliers of the control components. The recommendation to OEMs here is:

  • They should follow the latest standards in control technology to ensure the desired modularity and scalability.

  • Beyond the machine edge, interfaces should always be state of the art. This will give OEMs an optimally designed system. It will also ensure that they are well equipped for the future expansion of services based on digital services.

For other function groups, the advantages and disadvantages of customised interfaces should be systematically weighed up. The most important reasons for non-standardised interfaces:

  1. There are requirements from end users who want to consciously differentiate themselves from individual suppliers or focus on them.

  2. Differentiation from competitors through data-based business models such as after-sales, service and similar services.

  3. Consciously equipping modules with specific interfaces in order to set oneself apart from the competition. OEMs who see themselves as technology leaders in particular make use of these options.

  4. Use of sensors/actuators or combinations thereof that have been developed according to OEM specifications: Here, too, the protection of one's own know-how is the strongest motive for using customised interfaces.

Customisation options from HARTING

What customisation options does HARTING offer to implement customer-specific interfaces? Ranked by degree of customisation (ascending), these are:

  • The contact inserts can be combined with different housing types according to the modular principle. This results in easy scalability for the IP protection class, EMC protection or even the installation situation;

  • Cable entries and printing on enclosures can be freely configured and ordered to customer specifications using online configurators.

  • Assembly with contacts with different properties: this allows contact inserts to be designed to customer specifications.

  • Many contact inserts can be fitted with coding pins instead of contacts at individual locations.

  • Pin and socket combinations can be used for coding instead of fastening screws.

  • For data transmission, sections can be designed that are precisely tailored to the end user's environment; for this purpose, standardised preLink® contact blocks are used to create suitable connector types for different ends of the data lines in the required protection classes.

  • In modular connector systems, electrical contact inserts can be combined with other media such as pneumatics or fibre optics. The large number of available modules allows the creation of unique interfaces;

  • Products specified by the customer and assembled and tested by HARTING at the factory – from connector sets to individual cable assemblies.

  • At the highest level, interfaces are developed according to individual customer requirements – with the aim of meeting even the most unusual requests from customers in the mechanical and plant engineering sector.

References

  1. Megatrend: Customization

  2. Piller, F. T.; Stotko, C. M. (HRSG.): Mass Customization und Kundenintegration. Düsseldorf: Symposion 2003.

Jakob Dück

Jakob Dueck

Position: Industry Segment Manager Machinery

  • Department: Industry Segment Management
  • Company: HARTING Technology Group

Related news


Lights Out Manufacturing .png
10 December 2025 Products

Rethinking Connectivity for Lights-out Semiconductor Manufacturing

As chip complexity grows, innovations like edge computing and agentic AI are paving the way for “lights-out” manufacturing. This shift isn’t about eliminating humans, but about smarter resource use, real-time data insights, and sustainable processes.
read more
2022-09_Verschwommene Lichter_Stadt_Straße_GettyImages-615429200.jpg
9 December 2025 Products

Year in Review: Connectivity Trends Shaping 2025

As industries accelerate toward bringing new technologies to market, connectivity is emerging as a necessary catalyst for transformation. As we look back on the changes we saw across industrial connectivity, from hyperscale data centers to smart factories to modern power grids, here were the five trends that made the most impact ... and will continue making waves next year and beyond.
read more
Header_Product-News_Han-Contacts-on-Reel.jpg
5 November 2025 Products

Faster processing of turned contacts

HARTING is launching a solution that processes turned contacts on reel to speed up cable assembly in semi-automatic and fully automatic crimping machines. High-quality contacts can thus be crimped onto conductors in a matter of seconds.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590