2. News
  3. Innovative across generations
tec.news
20 November 2025
4 minutes

Innovative across generations


Connectors and adapters are everything. They connect devices and generations of technologies: the key to flexibility and innovation.
The adapter is king
Joachim Zellner

Joachim Zellner

Position: Managing Director

  • Company: ZVK GmbH
Andreas Klees

Andreas Klees

Position: Managing Director

  • Company: ZVK GmbH

The demands placed on modern data communication are constantly trending upwards - and with them the complexity of infrastructures. Connectors are at the heart of these developments: they not only connect devices, but also entire generations of technologies. The future does not belong to a one-size-fits-all solution, but instead to intelligent adaptation. Adapters are becoming the key to flexibility and innovation.

Consolidation and diversity – the current situation


The last few decades have been characterised by the pursuit of standardisation and convergence. Ethernet has established itself as the universal physical layer, enabling cross-sector communication. Cabling standards – predominantly ISO/IEC 11801 and EN 5073 – ensure a certain degree of uniformity, particularly in office and data centre environments, but also in industrial production. Nevertheless, it is clear that the variety of connectors and cabling philosophies in use is greater than ever before.

Infrastructure in transition: copper, fibre optics and the convergence to Ethernet


Infrastructure in transition: copper, fibre optics and the convergence to Ethernet

Today, infrastructure can be roughly divided into three areas: The connection of end devices to the local area network (LAN), which is mainly based on copper technology, transmission in wide area networks (WAN) and the connection of data centres, where fibre optic technology prevails. Despite these differences, there is a clear convergence at the physical layer: everything runs over Ethernet. However, this layer is diverse – wireless technologies are deployed to connect many end devices, but these are in turn connected to the access point by way of classic connectivity, usually RJ45.

In data centres, on the other hand, optical technology dominates with a large number of LC connectors for multiple fibres and MPO connectors for high packing densities and bandwidths.

In data centres, on the other hand, optical technologies prevail with LC duplex connectors with 2-fibre connections for transmitting and receiving (10/25G). MPO/MTP multi-fibre connectors for parallel optics are generally deployed for data rates of 40/100/200/400/800G/1.6T and high port densities.

The state of the art shows that Ethernet has resulted in a convergence of connectors, but the systems have evolved and grown historically and will continue to grow in the future. Adapters have become indispensable for connecting the systems of yesterday, today and tomorrow. Adaptation is no longer a necessary evil, but a strategic advantage, as it always involves Ethernet according to IEEE 802.3, thereby ensuring absolute data transparency in terms of communication.

The role of adapters – flexibility instead of a one-size-fits-all solution


Adapters are strategic infrastructure components enabling flexible connections between different systems. They ensure data integrity and future-proofing by supporting adaptation to new technologies and devices without restricting data transmission. The data lifeline does not require absolute uniformity at Layer 0. Far more, it is crucial to choose the right, future-proof connector for the respective application. Data integrity and consistency are not restricted by adapter cables – on the contrary: they enable flexible adaptation to new technologies and end devices, ensuring that the infrastructure remains usable for decades.

Network technology in transition: outlook for the future


The future in the area of end devices will not only be shaped by RJ45 – Single Pair Ethernet (SPE) will become more significant and bring new connectors into play. Here, too, adapters will be needed to ensure compatibility between old and new systems. Multi-fibre connectors are becoming increasingly significant in data centres, with the number of fibres and performance levels steadily on the rise. While LC duplex connectors as small form factors are now standard, very small form factor connectors such as SN or MDC are setting new standards in terms of miniaturisation and port density. The same applies to multi-fibre connectors, where the new and more compact types such as SN-MT and MMC are already finding their way into the data centres of hyperscalers and AI/HPC clusters. This means that the same Ethernet is being transmitted by way of ever-new connectors – and this is also giving rise to new adapter solutions.

The future of connectors in data centres lies in miniaturisation, while simultaneously boosting data rates. Very small form factor connectors will become particularly dominant in hyperscale data centres. Even if these new connectors do not immediately become established across the board, they will have a lasting impact on infrastructure. In this context, adapters will continue to play a central role, bridging the gap between old and new technologies.

Conclusion


The convergence of Ethernet-based data communication is a successful model. At Layer 0, however, the world remains colourful and diverse. The right selection and combination of connectors – supported by adapters – makes it possible to flexibly serve all the relevant applications and requirements. While standardisation remains important in order to create a certain foundation, the future belongs to diversity and adaptability. The adapter is king – and therefore remains indispensable for the future.

ZVK GmbH is a leading provider of solutions in fibre optic and network technologies. The medium-sized company develops and manufactures high-quality cabling systems, connectors and components for demanding and sophisticated applications in the industrial arena, data centres and telecommunications. Drawing on many years of in-depth experience, innovative products and tailor-made services, ZVK supports its customers in implementing powerful and future-proof network infrastructures.

Discover all articels of tec.news issue 49

Get involved in shaping the tec.news!


Your feedback helps us to tailor the magazine even better to your interests and needs.

Participate now
tec.news editorial team

tec.news editorial team

  • Company: HARTING Stiftung & Co. KG
[email protected]

Related news


Get involved in shaping the tec.news!
14 January 2026

Reader survey

What do you expect from a technology magazine – product knowledge, trending topics or completely new perspectives? Let us know.
read more
harting-web-header-ethernet-gast-0062-2500x1500px-20251029.jpg
21 November 2025

Ethernet: 50 years old, but still the gold standard

Around since the 1970s, but not a bit tired: how Ethernet keeps reinventing itself and forms the backbone for the latest trends.
read more
Focus on transition
21 November 2025

Focus on transition

Indian Railways is using data to get on track for carbon neutrality and better safety. Powered by HARTING.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590