2. News
  3. HARTING is featuring numerous innovations on InnoTrans 2024
Products
23 September 2024
2 minutes

HARTING is featuring numerous innovations on InnoTrans 2024


Ethernet networks are gaining increasing ground as onboard technology in railway applications. This calls for appropriate connectivity solutions that meet the demanding challenges of rail transport. At this year’s InnoTrans in Berlin, HARTING will be highlighting M8 solutions with the internationally standardised T1 Industrial mating face for Single Pair Ethernet transmission. Operator interfaces also play a vital role in the safe interaction between people and trains, as well as modular PCB connections that grant developers greater latitudes for innovative designs.
Operator interfaces

Operator Interfaces


Operator interfaces forge the bridge between man and machine in the onboard technology of rolling stock. They enable the control, monitoring and interaction in goods and passenger transport applications. At InnoTrans 2024, the Technology Group will be presenting robust and intuitive operator interfaces that increase productivity and safety in operations – representing an ideal addition to the HARTING har-port service interfaces for control cabinets and control panels.

All models are designed for installation in control cabinets and panels and are divided into two sizes:

1. The size for a housing cut-out with a diameter of 22.3 mm is suitable for applications in automation, mechanical engineering and robotics – in other words, for the production of rail transport technology.

2. The size for a housing cut-out with a diameter of 30.5 mm is designed for applications in the train itself. In addition to the industrial-grade housing interfaces, users now also benefit from reliable and robust operating elements from a single source.

Operating and Command Devices

Mini PushPull T1 Industrial


The Mini PushPull series connectors are characterised by their convenient, tool-free operation. Plugged in until a clearly audible click is heard – and the secure connection is readily ensured. They are the ideal choice for applications challenged by moisture, dust and vibrations. An additional locking mechanism, which can be sealed, prevents unintentional pulling strain.

The latest version of the modular principle incorporates the internationally standardised T1 Industrial plug-in face for the transmission of Single Pair Ethernet – the slim and sleek Ethernet entailing just two copper wires. The plug and appliance inlet are standardised in line with IEC 63171-6 and are therefore suitable for industrial use.

Mini PushPull T1 Industrial

har-flex® adapter


The versatile har-flex® adapters enable mezzanine PCB spacing of 20 to 40 mm, enabling maximum flexibility in electronics design! In combination with the compact, flexible and robust har-flexPCB connector series, users benefit from numerous options for their device designs. A flexible pin count from 12 to 80, combined with the wide range of mezzanine PCB spacings provides extensive design options. Fitted with a robust locking mechanism for the adapter, reliable handling is guaranteed.

har-flex® adapter

har-modular® cable connector


The new har-modular® modular connector system is now also available as a cable connector, enabling device designers to customize board-to-cable connections precisely according to their requirements. Customer-specific combinations of power, signal and data modules can be realised rapidly and conveniently. A wide selection of possible modules, which can be freely combined, saves unnecessary mould and tooling costs.

The online configurator enables users to select, configure and order the modules as required. All the necessary design related data is supplied automatically. Data and samples are available from a single source. The shell housings are available in ten different sizes for 1 to 10 modules, resulting in more than a billion possible combinations for a solid and DIN 41612-tested connection. This represents the ideal and flexible connection for applications on railway vehicles, on the tracks and in signalling cabins. Har-modular® meets the fire protection requirements of EN 45545-2.

har-modular® cable connector

More


Operator interfaces

Explore eShop

Discover our products for operator interfaces in the HARTING eShop.
Operator interfaces
PushPull

Explore eShop

Discover our HARTING PushPull product range in the HARTING eShop.
Learn more
har-flex Sigmatek

Explore eShop

Discover our har-flex® product range in the HARTING eShop.
Discover
har-modular.jpg

Explore eShop

Discover our har-modular® product range in the HARTING eShop.
Discover
Industrial Ethernet solutions

Industrial Ethernet

Learn more about the HARTING ethernet portfolio for industrial applications.
More

Jonas Diekmann

Jonas Diekmann

Position: Technical editor

  • Department: Global Product Management
  • Company: HARTING Electronics GmbH
[email protected]

Related news


Data Centre header background
23 October 2025

Building Smarter Data Center Infrastructure for the AI Age

Serving next-generation, AI-driven applications requires a dramatic rethink of traditional data center design. Data center infrastructure must evolve rapidly – becoming not only larger, but smarter, faster, and greener. Every connection system and square foot now counts in the race to keep up with exponential demand.
read more
Vertiv SmartIT Banner.png
21 October 2025

Vertiv and HARTING Unveil Data Center Rack Power Solution at OCP Summit

HARTING and Vertiv have teamed up to introduce a new rack power solution designed to simplify and accelerate data center deployment. The Vertiv PDB solution was launched at OCP Summit in San Jose, California
read more
Food processing and packaging machinery
29 September 2025

Miniaturisation of production systems: Just how far can you scale down?

In order to minimise the amount of material used and achieve cost savings, machines and other means of production are becoming increasingly compact. This is a trend that can be observed globally. But just how far can the condensation of individual functions and, along with it, miniaturization proceed in a sensible way? From experience and close cooperation with customers from a wide range of industrial sectors, HARTING as a manufacturer of industrial interfaces can share practical recommendations and experience. This enables manufacturers and users of production systems to discover and exploit the enormous potential of miniaturisation.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745
  • 粤公网安备 44049102496590