2. News
  3. PNO specifies HARTING ix Industrial® as new PROFINET interface
Products
2 July 2021
2 minutes

PNO specifies HARTING ix Industrial® as new PROFINET interface


The new PNO guideline Profinet Cabling and Interconnection Technology - Guideline for PROFINET Version 5.0 specifies the ix Industrial® mating face as a new standard for Ethernet applications. The guideline was officially published on June 29, 2021.
ix-board-to-cable

On June 29, 2021, the PROFINET User Organization (PNO) published the PROFINET Cabling and Interconnection Technology - Guideline for PROFINET Version 5.0 , a new set of rules for PROFINET-compliant cabling in industrial equipment, systems, and plants. Thanks to the ix Industrial® PROFINET are benefitting from an Ethernet interface that is significantly more compact and more robust than previous RJ45 solutions - a path to the miniaturised future. The ix Industrial® mating face for Ethernet transmission represents a key new component in the SPC "Specific Passive Components" section.

Consequently, manufacturers of PROFINET-compliant devices are now able to develop more compact devices on a secure and reliable basis and thereby save valuable installation space in the control cabinet. Given the 70% smaller ix Industrial® device socket compared to known RJ45 connections, the number of ports can be doubled for the same device size or, conversely, a device can be designed that is significantly more compact.

In addition to the miniaturisation and space savings that will become increasingly vital in the future, the HARTING ix Industrial® interface offers device manufacturers and users one thing in particular: A high-performance, reliable, and industrial-grade connector paving the way to the future.

Core properties


  • 5.000 mating cycles

  • Robust metallic lock

  • THR shield contacts

  • 360 degree shielding

  • Transmission up to 10Gbit/s

  • PoE/PoE+

  • 70% smaller device socket

Benefits for PROFINET users and manufacturers:

  • Reliable contact in case of shock and vibration

  • Fewer contact interruptions

  • Acoustic feedback during insertion signals secure locking

  • Simple, convenient handling excludes accidental loosening

  • New miniaturisation options

  • Secure transmission

Depending on the application, users can choose between a straight or an angled cable outlet. This means that even tight spaces in control cabinets will not present any problems. Catering to demanding environments, the ix Industrial® interface will also be available in IP65/67 protected PushPull housings as from the autumn.

Measurement technology manufacturers established on the markets are reliably supporting the ix Industrial® standard with a wide range of measurement technology.

More


HAN rectangular ethernet connector

Explore eShop

Discover our ix Industrial® product range in the HARTING eShop.
Discover

Jonas Diekmann

Jonas Diekmann

Position: Technical editor

  • Department: Global Product Management
  • Company: HARTING Electronics GmbH
[email protected]

Related news


Lights Out Manufacturing .png
10 December 2025

Rethinking Connectivity for Lights-out Semiconductor Manufacturing

As chip complexity grows, innovations like edge computing and agentic AI are paving the way for “lights-out” manufacturing. This shift isn’t about eliminating humans, but about smarter resource use, real-time data insights, and sustainable processes.
read more
2022-09_Verschwommene Lichter_Stadt_Straße_GettyImages-615429200.jpg
9 December 2025

Year in Review: Connectivity Trends Shaping 2025

As industries accelerate toward bringing new technologies to market, connectivity is emerging as a necessary catalyst for transformation. As we look back on the changes we saw across industrial connectivity, from hyperscale data centers to smart factories to modern power grids, here were the five trends that made the most impact ... and will continue making waves next year and beyond.
read more
Header_Product-News_Han-S-450-Plus.jpg
5 November 2025

Han® S 450 Plus: Reliable and powerful connector for energy storage systems

HARTING's battery connector series now supports up to 500 A for faster charging and discharging—ideal for high-performance energy storage without overheating.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590