Rolling stock benefits from weight reduction due to lighter connectors and cables
Energy efficiency and weight reduction are key trends in rail vehicle construction. Lightweight connectors and shorter cable runs can make a significant contribution to reducing the overall weight.
Manufacturers of railway vehicles continuously try to reduce the energy consumption per passenger-kilometre driven. In addition to increasing capacity utilisation and using drives that are more efficient, weight is one of the most important levers in this respect.
When you think of connectors, you might wonder how such small components can help to reduce weight. In railway engineering, connectors can be quite complex and heavy systems. Even minor adjustments can lead to a weight saving of a few kilograms. However, even small connectors can actually save a few kilograms per wagon if used in sufficient numbers.
Furthermore, optimised cable routing with short cable runs offers significant potential for weight reduction.
Web-Seminar ‘InnoTrans 2026 Review’
Missed InnoTrans 2026? Within this Web-Seminar we’re presenting a comprehensive overview of all the solutions showcased at InnoTrans.
50% weight and space savings for modular connections
With the introduction of the Han® 4 HPR, HARTING has expanded its Han® HPR range of industrial connectors to include a further housing size between 3 and 6. The HPR series is suitable for very harsh operating conditions where solutions that are shock- and vibration-resistant, as well as salt-spray-resistant, are required. Bogies are one example of this.
The new connector size 4 allows 50% weight savings (approx. 300g per connector) compared to the previous standard size 6. This is achieved, amongst other things, by replacing the module’s metal frame with a plastic version. The solution continues to meet high standards for durability and protection rating (IP68/IP69) and is certified in accordance with IEC 45545 and UL 1977.
Depending on the number of connectors per locomotive or wagon and the respective connector configuration, switching from size 6 to size 4 can result in a weight saving of several kilograms per wagon. Calculated over a 40-year service life, every kilogram saved can lead to savings of several thousand euros in energy costs. Size 4 features an integrated PE connection. With over 150 different connector inserts, it offers a future-proof solution.
With the Han® 4 HPR users save 50% weight and installation space
Connector modules can halve the size of the connector
It is not only smaller and lighter connector hoods and housings that can help to reduce the overall weight of the interfaces in railway vehicles. Choosing the right connector inserts can also influence the choice of connection solution.
The
Overall, the number of interfaces required per rail vehicle or railcar can be reduced. The connection technology is becoming smaller and lighter, meaning that more modules and module types than before can fit into a single connector.
Han® 4 HPR connector equipped with four Domino modules
Product sample Han-Modular®
Would you like to experience the next level of modular industrial connectors?
Request your free sample to get a first impression.
Plastic connectors for the interior of the railway vehicle
Switching from metal to plastic connectors in the interior of the vehicle, for example, inside of the locomotive for cabinet applications, is also an option to increase the energy efficiency.
Manufacturers have been able to reduce connector housing weight for trams and trains up to 50% between one generation and the next – this is the significant difference in weight between the classic Han® aluminium die-cast and the
Due to the modularity and the many different uses, the
Han® 1A and Han-Eco® high-performance plastic connectors according to common railway standards
Replacement of distribution boxes and shorter cable runs
The
The housing consists of two parts and, thanks to the counter-pressure frame and the circumferential internal seal, achieves protection class IP69K. The removable cover allows service teams to install the system from both inside the vehicle and from the outside. The cables can be easily routed through the wagon wall. This enables additional weight reduction due to short cable runs.
The counter-pressure frame and circumferential internal seal achieve protection class IP69K
40% weight savings compared to conventional data cables
Passenger information systems and other comfort systems are increasing the demand for higher data transmission capacity on board trains. More and more data cables need to be routed in an ever-increasing number of areas within the rail vehicle. Ethernet networks are becoming increasingly complex, as is the cabling infrastructure inside the wagon. This presents rail vehicle manufacturers with logistical challenges in both new trains and retrofit projects.
Single Pair Ethernet (SPE) is a high-performance data infrastructure for railway and stationary applications that is reduced to just two copper wires. Compared with conventional 8-wire data cabling, SPE offers significant advantages in terms of weight, space requirements, fire load and resource consumption.
Thanks to SPE cables, railway vehicle manufacturers can reduce weight by up to 40% compared with conventional data cables. This means that less weight needs to be accelerated during operation, resulting in lower energy costs. At the same time, SPE rail cables have a diameter that is up to 35% smaller, which helps to solve the additional problem of confined installation spaces. More data cables can be accommodated in narrow cable ducts, both in new installations and in retrofits.
Single Pair Ethernet (SPE) cables can save up to 40% weight and 35% space
UIC 552 alternative enables up to 10 KG weight savings per wagon
More efficient energy consumption and reduced complexity are major trends in the railway industry. Manufacturers of railway vehicles are always looking for ways to reduce the weight of their vehicles.
The Han® HPR TrainPowerLine replaces existing solutions such as UIC, power or Y-distributors for train busbars. The complexity of the application was reduced considerably at the customer's request: a uniform solution now replaces the many variants that were previously required for busbar construction.
The result of developing the TrainPowerLine is a uniform connector design for the entire underbody distribution of a train. The advantages are obvious and range from shortened installation times to more economical use of materials, weight reduction and standardised processes in assembly. It is tailored to modern trains running in a network and offers weight advantages of up to 10 kilograms per wagon compared to previous standards in the market. Very little space is required to reliably supply all the electrical equipment and systems of the train.
Typical environment for the Han® HPR TrainPowerLine are underfloor applications as an alternative to the UIC 552
Your benefits at a glance:
Smaller and lighter connectors allow space and weight savings of up to 50%
Weight saving achieved by replacing distribution boxes, which also results in shorter cable runs
Lighter underfloor distributors up to 10 KG less weight per wagon compared to the well-known UIC 552 interface
Up to 40% lighter cables compared to conventional data cables enabled by Single Pair Ethernet (SPE) data transmission
Sustainability thanks to a lower carbon footprint for the same technical functionality
Another very important solution HARTING was offering us is the VarioShell 34. We use it for the end of car jumper connections between cars. So, this solution allows us to transmit up to four megawatts through a very compact interface that has not been possible before with other connection solutions or only in a much bigger space and much more weight, much more cost than what we can now do with the VarioShell.
Raul Heinrich
Director of Electrical Engineering | Siemens Mobility