2. Machine Building Connectivity
  3. Semiconductor Manufacturing
  4. Front End Semiconductor Tool and Equipment Connectivity

Front End Semiconductor Tool and Equipment Connectivity

From lithography to deposition and etch, front end tools perform the most critical processes that create the circuits on silicon wafers. These steps include adding and removing materials on the wafer with sub-micron accuracy, demanding seamless connectivity across power, data, and signal interfaces to ensure uninterrupted operation and real-time communication.


SemiconductorManufacturing_FrontEnd.tif

There's no time for downtime.


In the ultra-complex world of semiconductor manufacturing, connectivity isn’t just a detail, but a critical safeguard for uptime, yield, and profitability.

With the cost of a 2nm wafer reaching $30,000 or more and target production of 40,000 wafer starts per month, leading edge fabs can’t afford downtime. Even a few minutes can translate into hundreds of thousands of dollars in lost revenue. For tool and equipment manufacturers, this means reliability and uptime are paramount, and high-speed, continuous monitoring is essential. 

Space is at a premium

As fabs push to put more equipment in the same — or less — space, compact, modular connectivity enables tool designers to deliver more power and data in less space.

This is why semiconductor tool and equipment manufacturers have turned to HARTING's compact and reliable connector solutions to maximize uptime and profits.

Our Semiconductor Manufacturing Expertise


Maximizing Throughput for Semiconductor Manufacturers [Case Study]

Compact, Robust Connectivity Solutions for Semiconductor Manufacturing Equipment

Better Connectivity in the Small Footprints of Semiconductor Manufacturing

gauge-simple-high-solid.svg

Improve uptime

Reliable power, data, and signal connectivity helps you avoid downtime.
Icon plug circle check

Maximize power without increasing footprint

Compact connectors let you do more in less space.
hourglass-regular.svg

Get online faster

Development cycles take years, but once you're ready to build there's pressure to get to production and market as quickly as possible.
handshake-regular.svg

Rely on a partner, not just a vendor

Co-designs and rapid prototyping help you get to market faster.
wrench-solid.svg

Improve serviceability

Modular connectors and cable assemblies help you resolve issues and get back online faster.
earth-americas-solid.svg

Global and local support

In-the-region, for-the-region manufacturing and support from a global supplier.

Front End Semiconductor Applications


Controls

Smarter controls start with smarter connectivity.

In semiconductor fabs, machine controls are the brains behind every process. Many OEMs build their own control systems to meet the unique demands of their tools. But custom doesn’t have to mean complicated.

Flexible, high-performance connectors streamline the design and assembly of control electronics, helping teams build faster, test more reliably, and scale with confidence.

The HARTING har-bus® 64 connector is a trusted PCB standard for control boards, offering robust signal integrity and proven reliability in high-density environments. Whether you're integrating sensors, actuators, or power modules, har-bus® 64 delivers the flexibility and durability needed to keep your control systems running flawlessly under 24/7/365 conditions.

har-bus 64 semiconductors.png
d-sub & ix semiconductor.png

Data & Signal From Sensors

Real-time data for real-time demands.

Semiconductor tools rely on a constant stream of real-time data — including temperature, vibration, pressure, and flow — to control, analyze, and optimize the process. These metrics are captured by sensors embedded throughout the equipment, often across multiple chambers that must communicate seamlessly with each other and with the fab’s master control systems.

In this environment, connectivity is the backbone of performance. When footprint is limited and uptime is critical, choosing the right connector provides a strategic advantage.

HARTING’s D-Sub connectors provide reliable data transfer for legacy systems. And the ix Industrial® interface offers a compact, high-speed alternative to RJ45 — delivering up to 70% space savings without compromising signal integrity.

Power

Power boxes for tools and systems.

In a fab, nothing runs without power. Every tool, chamber, motor, and sensor needs reliable power to operate. But as the power requirements of tools and equipment have increased, the available space for reliable, robust connectors has decreased.

HARTING meets this demand for more power in a smaller footprint with connectivity solutions such as the Han-Modular® and Han Q connectors and with custom cable assemblies to meet the most challenging power and space requirements.  

HAN Q - Features .png

More Semiconductor Resources


2023-05_GettyImages-1414159128-Production.jpg

Compact, Robust Connectivity Solutions for Semiconductor Manufacturing Equipment

Because the cost to build a fab is so enormous and the cost to operate cleanroom space is very high, fab owners and operators prioritize uptime, reliability, and space when it comes to choosing the equipment, or tools, they use for chip manufacturing.
Read more
Semi Conductor IMAGE .jpg

Maximizing Throughput for Semiconductor Equipment Manufacturers [Case Study]

How one major semiconductor equipment manufacturer decreased the size of their internal power distribution box and maximized power output with HARTING solutions.
Read the full case study
Han-B-IP67-Dockingframe.jpg

Steel Docking Frames for Harsh Environments

Robust docking frames allow for machine modules and tools to be docked automatically and entirely tool-free.
Learn more
HARTING at Semicon West 2025

7 Insights from SEMICON West

As complex and amazing as semiconductor manufacturing is, the fundamentals still matter. Flexibility, modularity, serviceability, and sustainability are all important aspects of wafer manufacturing equipment. All these topics are among the key takeaways from the biggest semiconductor industry event.
Read all expert insights

Better Connectivity in the Small Footprints of Semiconductor Manufacturing


From smartphones and smartwatches to autonomous vehicles and AI servers, semiconductor chips can be found in devices everywhere. To keep up with the demand for these chips, semiconductor manufacturing equipment must produce more chips without requiring more from existing facilities.

Increasing yield without expanding the equipment footprint requires smarter, more efficient machines.

Modular connectors simplify complexity. Just like HDMI replaced RCA cables in consumer electronics, modular industrial connectors consolidate multiple functions into a single interface.

Read the full article

Ready to Talk Connectivity Solutions for Semiconductor Manufacturing?


Personal information

Contact information

Company

Address information

0/2000

By submitting the form you will send your request. HARTING Technology Group will then get in contact with you.

If you also confirm your e-mail address in an e-mail sent to you, you can subscribe to regular HARTING updates about events, news, products, and applications. You can unsubscribe at any time.

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590