20% higher current carrying capacity and faster cable installation
The steadily rising demand for energy is one of the main challenges in rail vehicle engineering. HARTING is responding to this with a brand-new contact technology in a compact design.
The energy requirements of rail vehicles have risen steadily in recent years. A combination of comfort expectations, digitalisation, increases in speed, and safety regulations is posing even greater challenges for rail vehicle manufacturing.
HARTING is rising to these challenges and supporting railway engineers with
At the same time, we are constantly striving to further improve existing technologies. The new HanĀ® HC DoubleContact technology was developed to set new standards for high-current and high-voltage interfaces.
Web-Seminar āInnoTrans 2026 Reviewā
Missed InnoTrans 2026? Within this Web-Seminar weāre presenting a comprehensive overview of all the solutions showcased at InnoTrans.
20% higher power in the same space
As the global leading manufacturer for railway connectors and cables, HARTING can look back to decades of knowledge for high current / high voltage interfaces. Whether for inter-car jumper between wagons or between the locomotive and the wagons, the demand to transmit higher and higher power is always present.
Therefore, HARTINGās developers examined the proven HanĀ® HC Modular high-current contact inserts for potential improvements. The result is the new HanĀ® HC DoubleContact technology. Increased contact conductivity enables a 20% higher current-carrying capacity.
The smallest version can safely transmit 300 A at 2,000 V, while the largest can safely transmit up to 700 A at 4,000 V. Enough flexibility to meet future challenges.
The new contacts (front) offer up to 20% higher current carrying capacity compared with classic HC contacts (back)
Faster installation and less cable tension due to rotatable contacts
The thicker the cable, the harder it is to handle. The developers at HARTING have not only considered ways to increase current-carrying capacity, but also how to optimise the handling of high-current connectors and cables. It takes clever ideas to simplify the assembly process.
Rotatable contacts are the solution for reducing tension on the cable. The new high-current contacts snap into the insulating body and can then be rotated into the correct position. This allows the installer much greater flexibility in cable routing compared to traditional HC contacts. The module frame can be secured with fewer screws, saving additional time during installation.
Work on high-current connections must be performed safely to prevent the risk of electric shock. The new high-current contacts feature comprehensive finger protection on both sides. This ensures a safe working environment during installation and maintenance processes.
Increased safety: HanĀ® HC DoubleContact with finger protection
Your benefits at a glance:
Up to 20 % higher current carrying capacity compared to actual HC contacts
Fast and easy installation due to efficient coding system, rotatable contacts and less components for the frame
Increased safety thanks to finger-protected contacts on both sides
High flexibility due to modular design: suitable for high power applications across different industries
What other customers say:
Suppliers have to continue to listen to our new requirements and new technical challenges and meet them with inhouse technical expertise to develop new products with testing capabilities like we do today. HARTING has been good at that and I think we should continue to build on that the same way.
Raul Heinrich
Director of Electrical Engineering | Siemens Mobility