HARTING Joins NVIDIA MGX Ecosystem to Power Next-Generation AI Infrastructure
HARTING Technology Group, a leading global provider of industrial connectivity, today announced it has joined the
As AI workloads grow and compute density increases, data centers must manage significantly more power within increasingly dense environments without compromising reliability, efficiency or scalability. That shift is placing new demands on the connectivity systems that deliver power to AI compute infrastructure.
“AI is fundamentally changing data center infrastructure, and HARTING has the engineering expertise to help enable that transformation,” said Philip Harting, Chairman of the Board and CEO, HARTING Technology Group. “Our inclusion in the NVIDIA MGX ecosystem brings our decades of connectivity experience in high power environments, from rolling stock to automotive, to the infrastructure supporting the next generation of AI.”
For the NVIDIA MGX platform, HARTING provides a 100A/480VAC power whip for the 3RU 110kW power shelf for NVIDIA Vera Rubin NVL72, supporting the transition to 800 VDC with a next-generation 157A/800 VDC DC-DC power whip connecting the power infrastructure to the compute rack.
“As AI compute becomes more powerful and rack densities increase, the industry has to rethink power distribution from the ground up,” said Christian Gysin, Chief Technology Officer and Member of the Executive Board, HARTING Technology Group. “The transition from 480VAC toward 800 VDC is a significant step in that evolution. Connectivity must support higher power levels while delivering the reliability, safety and scalability these environments demand. That is precisely where HARTING’s engineering expertise comes into play.”
HARTING solutions transmit power, data and signal across mission-critical systems worldwide. The company is drawing on decades of experience in demanding industrial environments and its global engineering and vertically integrated manufacturing capabilities to address the evolving connectivity requirements of AI infrastructure and data centers.
As part of the NVIDIA MGX ecosystem, HARTING will be featured on the NVIDIA AI Factory MGX Ecosystem wall at the OCP Global Summit 2026. The executives from HARTING will honourably attend the NVIDIA MGX ceremony. Besides, two HARTING power whip solutions supporting the NVIDIA Vera Rubin NVL72 platform will also be on display in the HARTING booth (Booth No. C79) demonstrating the power connectivity behind current and next-generation AI infrastructure.
Dipl.-Journ. Marco Stapelmann
Position: Head of Corporate Communication
- Department: Corporate Communication & Branding
- Company: HARTING Stiftung & Co. KG