2. News
  3. HARTING UIC IT circular connectors for fast and robust Ethernet and new solutions for power supply on trains
Products
23 September 2024
5 minutes

HARTING UIC IT circular connectors for fast and robust Ethernet and new solutions for power supply on trains


HARTING expands the UIC family with the UIC IT circular connector.
Hero_UIC_IT_News.jpg

HARTING has expanded its UIC-compliant portfolio to include a series of future-proof IT versions for the transmission of Gigabit Ethernet. The new interfaces are called HARTING UIC IT and differ in their arrangement of contacts: They offer space for 8, 8+16 (acc. to IRS 50558) or 8+8 poles. This means they can transmit data and signals for door control or Gigabit Ethernet for passenger information systems, for example.

The inserts in the new series are based on the proven Gigabit modules from the Han-Modular® series. Ethernet transmission up to Cat. 8 is possible with these robust and powerful connector components. The new series therefore fulfils the requirements of an Ethernet infrastructure for rail vehicles with a higher bandwidth.

The HARTING portfolio in this segment previously consisted of UIC 558 interfaces with 13, 18 and 23 contacts. Based on the UIC 558 housing, HARTING has also created a further solution (70 A/500 V) for the power supply in trains with UIC POWER70. A backshell increases robustness by sealing the device socket from behind. The new connector achieves protection class IP69, so that plugs and sockets can be easily installed outside the vehicle body. The UIC POWER70 therefore goes beyond the circular connector solutions that were previously available on the market.

The new UIC family members: HARTING UIC IT - Sufficient transmission capacity for Cat. 8 Ethernet communication on trains and HARTING UIC POWER70 - High environmental protection for outdoor power transmission up to 70 A

The new products fulfil other relevant railway standards: These include IEC 61373, category 2, which ensures an increased protection against shock and vibration. The materials used also fulfil the fire protection requirements according to IEC 45545 (class: R22/R23, HL1-3) and are flame retardant according to UL 94 V-0.

A special feature of the UIC series is a breakaway safety function. If two electrically non-separated vehicles inadvertently move apart, the safety mechanism ensures that both sides of the interface release automatically and non-destructively above a defined tensile force. With UIC POWER70, the signal contacts are used to switch off the power contacts to ensure the safe and non-destructive separation.


Benefits at a glance:


  • Breakaway function: This safety function ensures the non-destructive separation of plug and socket when electrically connected vehicles are moved apart

  • High degree of protection IP67/IP69 for the application

  • 10,000 mating cycles guarantee a long service life

  • All interfaces are available as ready-made assemblies

  • An additional functional earth increases the safety of the UIC POWER70 application

Nils Doekel

Nils Dökel

Position: Group Leader, Industrial Circular Connectors

  • Department: Product Management Installation Technology
  • Company: HARTING Technology Group

Related news


Lights Out Manufacturing .png
10 December 2025

Rethinking Connectivity for Lights-out Semiconductor Manufacturing

As chip complexity grows, innovations like edge computing and agentic AI are paving the way for “lights-out” manufacturing. This shift isn’t about eliminating humans, but about smarter resource use, real-time data insights, and sustainable processes.
read more
2022-09_Verschwommene Lichter_Stadt_Straße_GettyImages-615429200.jpg
9 December 2025

Year in Review: Connectivity Trends Shaping 2025

As industries accelerate toward bringing new technologies to market, connectivity is emerging as a necessary catalyst for transformation. As we look back on the changes we saw across industrial connectivity, from hyperscale data centers to smart factories to modern power grids, here were the five trends that made the most impact ... and will continue making waves next year and beyond.
read more
Header_Product-News_Han-Contacts-on-Reel.jpg
5 November 2025

Faster processing of turned contacts

HARTING is launching a solution that processes turned contacts on reel to speed up cable assembly in semi-automatic and fully automatic crimping machines. High-quality contacts can thus be crimped onto conductors in a matter of seconds.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590