2. News
  3. IEC Ethernet standards: The primary element empowering the AES
tec.news
29 November 2024
3 minutes

IEC Ethernet standards: The primary element empowering the AES


Data and power are the foundations of an All Electric Society (AES). In an electrified world, there is no device that can function without the appropriate power supply and communication. This communication between all participants is the key to sustainable energy generation and the necessary efficiency gains. While international Ethernet standards already ensure data communication today, power supply solutions are highly fragmented across the individual sectors of the AES.
IEC Ethernet standards: The primary element empowering the AES

The reliable transmission of power and data plays a central role in the All Electric Society (AES). The vision of a fully electrified and digitalized society and the networking of industrial processes are key components in this context. This calls for uniform standards in the transmission of both lifelines in order to harmonise the individual sectors of the AES in an expedient way.

International IEC standards for Ethernet have long been established in data transmission, but this standardisation is still pending when it comes to power. The amount of data to be transmitted is growing exponentially and the power supplies must break new ground in terms of regenerative energy generation. The associated challenges for adequate connection technology are our HARTING’s incentive.

Efficiency gains through data networking


The efficiency gains required for the AES can only be achieved through comprehensive and extensive networking. Energy generation and consumption must be seamlessly attuned to each other. Whether through the use of Ethernet via two, four or six copper wires - uniform standards for protocols, for the cable infrastructure and for interfaces have long since covered the major share of industrial communication. Ethernet standards are essential for models such as the Digital Twin and an Asset Administration Shell (AAS).

Just like the flow of data, energy transmission must also become convergent. At present, however, it is still being conceived as a unidirectional distribution. The data lifeline is becoming the leading element for energy on the course to standardised and networked solutions. Integration of power and data Connecting devices via mains adapters is time-consuming and inefficient. In fact, it is a step backwards to the power distribution of a pre-digital age. Meanwhile, more and more end devices are demanding innovative power solutions.

Integration von Power und Data


Data is a role model here, as it always flows bidirectionally. Consequently, it was logical to consider the power supply from the data side, which gave rise to standardised systems such as Power over Ethernet (PoE) and Power over Data Line (PoDL).

Future-proof hybrid interfaces


In the case of devices with higher power requirements, it also makes sense to consider the power supply from the data side, because in a digitalised world, the data connection is becoming the key standard. This is creating new interfaces in industrial automation, in which data connectivity is being further developed around the topics of energy as part of a hybrid interface. Here, the "new" energy follows the data; the "new" energy is usually not always an AC grid, but potentially also DC voltage.

The future of data and power integration


The network connection and the power connection are equally important for the AES. The future is characterised by data, as is enabled by Ethernet and the standardisation committees. This effective approach will be supplemented in future by building a bridge to energy. HARTING is involved when it comes to thinking about power for data transmission. This opens up scope for innovations. New interfaces and hybrid connection concepts are emerging, which are driving data and energy forward together.

»

The first goal is to consistently place power under the control and management of data in order to achieve intelligent device power. And the decisive step to follow will be to offer one single cable for both lifelines – the One Cable Solution.

Portrait_Jonas_Diekmann_HARTING.jpg

Jonas Diekmann

Technical editor HARTING Electronics

Jonas Diekmann

Jonas Diekmann

Position: Technical editor

  • Department: Global Product Management
  • Company: HARTING Electronics GmbH
[email protected]

Related news


Get involved in shaping the tec.news!
14 January 2026 tec.news

Reader survey

What do you expect from a technology magazine – product knowledge, trending topics or completely new perspectives? Let us know.
read more
harting-web-header-ethernet-gast-0062-2500x1500px-20251029.jpg
21 November 2025 tec.news

Ethernet: 50 years old, but still the gold standard

Around since the 1970s, but not a bit tired: how Ethernet keeps reinventing itself and forms the backbone for the latest trends.
read more
Focus on transition
21 November 2025 tec.news

Focus on transition

Indian Railways is using data to get on track for carbon neutrality and better safety. Powered by HARTING.
read more

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590