Country flagChina Mainland

Industrial Connectors High Power Connectors Circular Connectors M12 System Cabling har-modular®: PCB Connectors
News Room Press & media contacts Technology magazine tec.news
PEOPLE. POWER. PARTNERSHIP. Jobs Your Contact Persons
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
  2. Wind Energy
  3. Plug connectors increase the value of wind energy investments

Plug connectors increase the value of wind energy investments

In the long run, components which simplify installation and maintenance of a wind turbine can improve the value of the plant enormously. Learn how!


DOWNLOAD FREE WHITE PAPER
SIMPLIFY CABINET CONSTRUCTION
Plug connectors increase the value of wind energy investments

The value of a wind turbine (WT) is not only measured by the investments into machines and site development, but also in the way it is used over the whole lifetime. In the long run, components which simplify installation and maintenance can improve the value of the plant enormously. If a wind turbine manufacturer uses pluggable connectors for the electrical connections between WT modules, this can lower both the investment costs (CAPEX) and the operational costs (OPEX).

Easy installation and maintenance of wind turbines


A good example of a regularly replaced component on a wind turbine is the slip ring – the interface between the stationary nacelle and rotating hub. The slip ring is used to transmit the signals for the pitch systems that determine the angle of incidence of the rotor blades.

This interface can have a pluggable design: HARTING’s solution uses Han-Modular® inserts and the Han-Modular® hinged frame.

The plug solution offers many advantages over permanently attached wiring. The slip ring can be replaced more quickly, thereby reducing downtimes. During maintenance in the service workshop, the slip ring can be replaced without intervention in the pitch system and without dismantling the connecting cables. The service fitters in the nacelle do not require special tools. This reduces costs for maintenance and repair.

Slip-ring connection at a wind turbine

Investment costs under control


There are good cost-saving opportunities associated with using plug connectors for the initial investments as well as the installation costs. Power cabinets in the wind turbine are still mostly hardwired. They are hardwired and tested during assembly in the factory, then the connections are disconnected and restored at the system level in order to repeat the process after a further disconnection in the field. The use of pluggable connectors speeds up the installation process and increases the modularity of the WT. The pluggable connectors also open up options for the modularisation of the power cabinets.

Icon_Whitepaper-Wind-energy.png

Connectivity in Wind Turbines

This PDF White Paper will show you how connectors could increase the efficiency of wind turbines and reduce the CAPEX and OPEX. (PDF | 5 MB | 22 pages)

Request free white paper

Levelized cost of electricity


The value of pluggable connections for installing and operating a wind turbine can be illustrated with numerous other application examples.

The adjacent diagram shows the areas in which plug connectors simplify and thereby enable savings in installation/investment (CAPEX) and operations (OPEX). It is worth highlighting that significant savings can be made using plug connectors even in the investment phase, with assembly and installation in the field.

This reduces the costs for installation of wind parks by shortening assembly processes. Plug connectors help any installation fitter who must attach components at inaccessible angles in the nacelle and tower.

In the long run, an evaluation of costs incurred for capital goods in a WT cannot avoid the use of pluggable connectors. The initial costs for these connectors, which incur less than 0.5% of the total investment, will already be amortised after just a few maintenance processes.

Apart from this, the installation logistics would quickly reach their limits at current conventional plant sizes (onshore average: 3.3 MW) without a modular design that uses plug connectors.

Levelized cost of electricity

Levelised costs of electricity

Your benefits at a glance:


  • Savings of time and cost due to rear mounting options

  • Separate pre-assembly of entire cable harnesses possible

  • Reduction of manufacturing cost by better division of labour

  • Additional time savings by using Han® ES Press rapid termination

»

We believe that our suppliers are long-term partners, from last one decade we are working with HARTING. And particularly for India, we have started working with HARTING from 2021 and we’re using different, 80 types of connectors from HARTING, which is used in our nacelle and hub. HARTING offer the robust design, the high-quality product with performance and with sustainability, and also with use very ease to maintenance, as it is plug & play.

portrait_Prafullamkumar_Dhole__900x900.tif

Prafullakumar Dhole

Head of Procurement | Senivion

White Paper Download


Learn how connectors can increase the efficiency of a wind turbine and reduce the CAPEX and OPEX costs.

Personal information

Contact information

Please enter your phone number with country code and area code. Ex. +1 123-456-7890.

Company

Address information

By submitting the form you will send your request. HARTING Technology Group will then get in contact with you.

If you also confirm your e-mail address in an e-mail sent to you, you can subscribe to regular HARTING updates about events, news, products, and applications. You can unsubscribe at any time.

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590