2. Machine Building Connectivity
  3. Semiconductor Manufacturing
  4. Semiconductor Manufacturing Subfab Connectivity

Semiconductor Manufacturing Subfab Connectivity

Beneath the pristine environment of a semiconductor cleanroom lies the subfab and the critical infrastructure layer housing machines such as power distribution units, vacuum pumps, abatement systems, chillers, and gas delivery units. These systems are essential for maintaining process integrity, safety, and uptime. Reliable connectivity across power, data, and signal is vital to ensure these machines function seamlessly and communicate reliably with the tools in the cleanroom above..


SemiconductorManufacturing_SubFab.tif

Reliable power supply keeps fab infrastructure online.


The subfab is where the real orchestration of semiconductor manufacturing happens, and its complexity rivals the fab itself. In addition to supporting the process tools and equipment, subfab systems are also critical for ensuring the efficiency and safety of the fab.

In the subfab, connectivity solutions that provide high-speed data transfer and reliable power distribution are key for supporting mission-critical equipment and systems.

Billions at stake: Building a leading-edge fab can cost $10–$20 billion, making uptime and reliability non-negotiable.

Energy-intensive operations: A single fab can consume 100 megawatts or more of power each hour, equivalent to powering a small city.

Thousands of systems to manage: The subfab contains vacuum pumps, gas delivery, chemical systems, cooling, and other critical infrastructure, all running in harmony 24/7/365.

HARTING’s connector portfolio is built for this environment by offering:

  • Plug-and-play flexibility to simplify installation and reduce downtime

  • Rugged construction for continuous delivery of high voltage and current

  • Custom cable assemblies to meet your specific power, footprint, and environmental requirements

Semiconductor Fab Connectivity


Front End Equipment Connectivity

Inspection & Testing Connectivity

Back End Equipment Connectivity

angles-up-solid (1).svg

Ensure reliability

Choose the most dependable components for subfab applications.
gears-solid.svg

Hold up in demanding environments

Maintain the highest level of performance, even under strenuous operating conditions.
wrench-solid.svg

Reduce downtime

Repair and replace parts instantly with easy-to-swap modular connectors and cable assemblies.

Subfab Connectivity Applications


Han for PDUs.png

Power Delivery

Meet the never-ending demand for more, always-on, high-voltage power.

If a subfab is the brains for semiconductor manufacturing, the Power Distribution Units (PDUs) serve as the nerve center, routing energy to thousands of components that must operate in perfect sync at all times.

A single hour of power disruption can cost fabs millions of dollars in lost productivity so power connectors must withstand continuous use without compromising performance.

HARTING’s Han-Modular®, Han-Power®, and Han-Eco® connectors simplify PDU integration, reducing installation time, labor costs, and risk of error. With hybrid or modular connectors, one connector can deliver both power and data, streamlining design and reducing footprint.

Vacuum Systems

Precision under pressure.

Vacuum systems regulate pressure, remove contaminants, and enable precise environmental control across multiple chambers. These systems must operate continuously and flawlessly to support the cleanroom and wafer production.

Vacuum pumps, valves, and sensors must communicate in real-time with master control systems. Rugged, modular connectors like Han-Modular® and ix Industrial® simplify installation and reduce maintenance time — delivering secure, high-speed connections that keep vacuum systems running 24/7 with minimal risk and maximum reliability.

Hybrid connectors for vacuum systems.png
Datacenter_Gebaeudemanagement_Lighting.tif

Lighting, HVAC & Security Systems

Connectors make lighting, HVAC, and security systems more efficient, contributing significantly to energy savings and operational effectiveness.

Connectors facilitate easy installation and replacement of lighting and HVAC components by allowing for quick connect and disconnect capabilities. This reduces downtime during maintenance activities, ensuring that systems remain operational and that energy isn't wasted due to prolonged outages.

Other benefits include:

✓ The adaptability of connectors provides design flexibility and future modification without requiring rewiring or system overhauls
✓ Smart connectivity enables real-time monitoring and adjustments to optimize energy usage
✓ Secure, reliable connectivity leads to improved uptime and utilities cost savings
✓ Efficient systems reduce carbon footprint of facilities, aligning with sustainability goals and regulations

More Semiconductor Resources


2023-05_GettyImages-1414159128-Production.jpg

Compact, Robust Connectivity Solutions for Semiconductor Manufacturing Equipment

Because the cost to build a fab is so enormous and the cost to operate cleanroom space is very high, fab owners and operators prioritize uptime, reliability, and space when it comes to choosing the equipment, or tools, they use for chip manufacturing.
Read more
Semi Conductor IMAGE .jpg

Maximizing Throughput for Semiconductor Equipment Manufacturers [Case Study]

How one major semiconductor equipment manufacturer decreased the size of their internal power distribution box and maximized power output with HARTING solutions.
Read the full case study
Han-B-IP67-Dockingframe.jpg

Steel Docking Frames for Harsh Environments

Robust docking frames allow for machine modules and tools to be docked automatically and entirely tool-free.
Learn more
HARTING at Semicon West 2025

7 Insights from SEMICON West

As complex and amazing as semiconductor manufacturing is, the fundamentals still matter. Flexibility, modularity, serviceability, and sustainability are all important aspects of wafer manufacturing equipment. All these topics are among the key takeaways from the biggest semiconductor industry event.
Read all expert insights

Better Connectivity in the Small Footprints of Semiconductor Manufacturing


From smartphones and smartwatches to autonomous vehicles and AI servers, semiconductor chips can be found in devices everywhere. To keep up with the demand for these chips, semiconductor manufacturing equipment must produce more chips without requiring more from existing facilities.

Increasing yield without expanding the equipment footprint requires smarter, more efficient machines.

Modular connectors simplify complexity. Just like HDMI replaced RCA cables in consumer electronics, modular industrial connectors consolidate multiple functions into a single interface.

Read the full article

Ready to Talk Connectivity Solutions for Semiconductor Manufacturing?


Personal information

Contact information

Company

Address information

0/2000

By submitting the form you will send your request. HARTING Technology Group will then get in contact with you.

If you also confirm your e-mail address in an e-mail sent to you, you can subscribe to regular HARTING updates about events, news, products, and applications. You can unsubscribe at any time.

HARTING Newsletter

Social Media

Country flagChina Mainland

© HARTING Technology Group | HARTING (Zhuhai) Manufacturing Co., Ltd. Room 201, No.19 Chuangxin Si Road, Zhuhai City Tel: 86 40 01761166 Shanghai branch Room 3501-3510 Grand Gateway 1, NO.1 Hong Qiao Road, Shanghai Tel:86 21 34189758

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Privacy Policy (Umeng+)
  • Terms of Use
  • Customer Information
  • 粤ICP备19078745号-1
  • 粤公网安备 44049102496590